DIO#.DIR

Description

Sets or whether the bi-directional IO is an input or output.

Value Description
0 The bi-directional IO is treated as an input signal
1 The bi-directional IO is treated as an output signal

Examples

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0 (input)
Data Type Integer
See Also  

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDO Mappable
EtherCATClosedEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DIO1.DIR 0x368A 0x1 USINT - - RW False
DIO2.DIR 0x368B 0x1 USINT - - RW False
DIO3.DIR 0x368C 0x1 USINT - - RW False
DIO4.DIR 0x368D 0x1 USINT - - RW False
DIO5.DIR 0x368E 0x1 USINT - - RW False
DIO6.DIR 0x368F 0x1 USINT - - RW False